AOUT#.SOURCE
Description
This keyword sets the source of the analog output
| Value | Description |
|---|---|
| 0 | AOUT#.VALUE is driven by AOUT#.VALUEU. |
| 1 | AOUT#.VALUE can be driven by an action in the Action table |
| 2 | AOUT#.VALUE is driven by the associated fieldbus object |
Examples
Usage
When AOUT#.SOURCE = 0 (User), then AOUT #.VALUE will be controlled by AOUT #.VALUEU.
When AOUT#.SOURCE = 1 (Action table), then AOUT #.VALUE will be controlled by the assigned action, if any.
When AOUT#.SOURCE = 2 (Fieldbus
A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design), then AOUT#.VALUE will be controlled by the associated fieldbus analog output object 3800h sub 2.
Code
Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:
--> AOUT1.SOURCE 0 (User) --> AOUT1.VALUE 0.000 V --> AOUT1.VALUEU 1 --> AOUT1.VALUE 1.000 V --> AOUT1.SOURCE 1 --> AOUT1.VALUE 0.000 V
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added fieldbus source | 02-00-01-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 2 |
| Default Value | 0 |
| Data Type | Integer |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
|
Copyright © 2018 Kollmorgen |
|